Setting parameters for an KNX device - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 13.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > KNX Vendor Integration
Document type
Application Note
Document number
LIT-12013148
Version
13.0
Revision date
2023-10-18

Procedure

  1. Use a web browser to log on to the network engine's UI.
  2. Select the device object in the Network Tree.
  3. Switch to the Details view of the device and click the Hardware tab.
  4. Click the link in the Vendor Configuration Data field to modify the parameters shown in the following table.
    Table 1. Field device parameters

    Parameter

    Value

    [1]

    Represents an IP address that is dependent on the connection mode (parameter 2).
    • If parameter 2 is set to N, you must set parameter 1 to the IP address of the KNX IP device.
    • If parameter 2 is set to Y, you must set the IP address to the multicast address used in the KNX routers. The standard KNX multicast address is 224.0.23.12.

    [2]

    Represents the connection mode of the device.
    • Tunneling mode is N.
    • Routing mode is Y.
  5. Click SAVE.