About this task
Important: Each KNX IP Gateway has
its own unique IP address. Specify the IP address only once for the network engine.
Procedure
- Use a web browser to log on to the network engine's UI.
- Select the KNX Integration object in the Network Tree.
- Click the + icon (Add Network Item) to create the item.
- In the Create Item wizard, select Field Device from the General Type drop-down and select Manual.
- Select VND Controller from the Object Type drop-down.
- Review the unique identifier in the Unique Identifier field and change it.
- Click NEXT.
- Click CREATE.