Inserting a VND integration using SCT - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 13.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > KNX Vendor Integration
Document number
LIT-12013148
Version
13.0
Revision date
2023-10-18

Procedure

  1. Use the Launcher to log on to SCT. If you need to install the Launcher, refer to Launcher Installation Instructions (LIT-12011783).
  2. From the Insert menu, select Integration.
  3. In the Insert Integration Wizard, select VND Integration under Select Object Type and click Next.
  4. In the Destination window, select an engine.
  5. In the text field to the right of the Identifier area, enter a unique identifier value. Click Next.
  6. In the Configure window, click the Hardware tab. In the Vendor Driver field, enter the name of the driver according to Table 1.
    Note: The Vendor driver file name is case sensitive. Enter only one driver name.
    Note: Change all driver file names from *.so to *.so.signed, if you upgrade a SNx device to Release 11.0.2 and later with the KNX VND integration already installed.
    Table 1. Vendor driver file name to use

    Network engine

    First driver

    Second driver

    NCE25, NAE35, NAE45, NAE55, NIE59

    libKNXDriver.so

    -
    SNExxxxx, SNCxxxxx libKNXDriver.so.signed -

    NAE85, OAS

    KNXDriver.dll

    KNXDriver_1.dll

    Note: Do not modify the Vendor Reference field; it is not used in this integration.
  7. Click Next.
  8. Click Finish.
  9. Click Done.