Requirements - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 13.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > KNX Vendor Integration
Document number
LIT-12013148
Version
13.0
Revision date
2023-10-18

To add a KNX integration as a VND integration, you must have the following:

  • A properly configured KNX system to communicate with KNX IP interfaces and KNX IP routers. All KNX line devices must be properly installed and communicating with KNX IP devices (interfaces and routers) before you add the integration in SCT and Metasys UI.
  • The KNX IP interfaces and KNX IP routers connected correctly to the network engine.