Summary of changes - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 12.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Brand
Metasys
Product name
KNX Vendor Integration
Document type
Application Note
Document number
LIT-12013148
Version
12.0
Revision date
2022-05-20
Language
English

The following information is new or revised for Metasys 12.0:

  • Updated Inserting a VND integration to include a note to change all driver file names from *.so to *.so.signed, if you upgrade a SNx device to Release 11.0.2 and later.
  • Updated Inserting a VND integration to include the new driver names for SNx devices.
  • Updated Serial port capture to document support of the USB to RS485 converter connection type.
  • Updated Diagnostic files and support to include information about Ethernet capture and updated USB port capture.
  • Added new section Ethernet capture to document how to capture diagnostic traces through an Ethernet connection.
  • Removed references to the NIE29, NIE39 and NIE49 because they are discontinued.