Overview - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 12.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Brand
Metasys
Product name
KNX Vendor Integration
Document type
Application Note
Document number
LIT-12013148
Version
12.0
Revision date
2022-05-20
Language
English

Network engines are Ethernet-based, supervisory engines that connect BAS networks to IP networks. You can monitor and control BAS field devices from a computer using the Launcher application. Install Launcher version 1.7 on your computer. Refer to the Launcher Installation Instructions (LIT-12011783) .

The SNC combines the network supervisor capabilities and IP network connectivity of SNE network engines with the Input/Output (I/O) point connectivity and direct digital control capabilities of equipment controllers. The network engines provide scheduling, alarm and event management, trending, energy management, data exchange, and password protection. They have the current release of Metasys system software pre-loaded at the factory.