Introduction - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 12.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Brand
Metasys
Product name
KNX Vendor Integration
Document type
Application Note
Document number
LIT-12013148
Version
12.0
Revision date
2022-05-20
Language
English

This document describes how to add, configure, and commission a KNX integration for a network engine. The KNX integration feature is supported on the following network engine series and software releases:

  • SNE and SNC series, which have supported the KNX integration feature since their introduction at 10.1
  • NIE59 series
  • NCE25, NAE35, and NAE45 series that have been upgraded to 9.0.7 or later
  • NAE55xx-2, -3 series that have been upgraded to 10.0 or later
  • NAE85 and LCS85 that have been upgraded to 10.0 or later
  • OAS from Release 11.0 or later

This document also describes how to upgrade an NIE59 at Release 9.0 to Release 12.0, to maintain the KNX integration capability.

Note: You can also commission an LCS85 server to use the KNX protocol. The steps are identical to those described in this document, with the selection of an LCS85 instead of an NAE as the primary difference. Where reference is made to an NAE85, the information is also valid for an LCS85.
Note: There are no modifications required when you upgrade from Release 10.0 to Release 10.1.

This document does not describe how to mount, wire, or power on an NAE, NIE, SNE, or SNC, how to build or download an archive database for a Metasys system site, or how to configure an NAE, NIE, SNE, or SNC to monitor and control a Building Automation System (BAS).