About this task
Note: USB drive capture is
available only for NAE85s and OAS.
Procedure
- Insert a USB flash drive into the USB drive on the NAE85 and OAS. Wait two minutes for the flash drive to initialize.
- Drag the KNX integration object from the navigation panel to the display panel, and then click the Hardware tab.
-
Click Edit, and then click the
browse button to open the Vendor Configuration Data
parameter list. In the Modify List dialog box:
- Set parameter 1 to Y.
- Set parameter 3 to the drive letter assigned to the USB flash drive.
See Figure 1 for an example.Figure 1. USB drive diagnostic example
- Click OK to save your changes, close the dialog box, and then click Save on the Hardware tab to save the KNX integration object. Diagnostic mode begins.
- Capture data for approximately ten minutes, then disable diagnostic mode by again opening the Vendor Configuration Data parameter list. Set parameter 1 to N and save the change.
- Remove the flash drive from the USB drive.
-
Review the log file by using a text editor. The log file includes all the
information related to the integration and communication traffic in hexadecimal
format.
Note: The diagnostic capture file is stored to the flash drive. The name of the text file is: KNXDriver‑<year><month><day>T<hour><minute><second>.log. For example, KNXDriver-20181004T144500.log.