Inserting a VND integration - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 12.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > KNX Vendor Integration
Document type
Application Note
Document number
LIT-12013148
Version
12.0
Revision date
2022-05-20

About this task

To insert a VND integration, complete the following steps:

Procedure

  1. Use the Launcher to log on to the network engine's SMP. If you need to install the Launcher, refer to the Launcher Installation Instructions (LIT-12011783).
  2. Drag the network engine device object from the navigation panel to the display panel. The Focus tab screen appears.
  3. Click . The Insert Integration wizard appears.
  4. In the Select Object Type window, click VND Integration, and then click Next.
  5. In the Destination window, click the network engine object, and then click Next.
  6. In the Identifier window, enter a unique name for the integration trunk, and click Next.
  7. In the Configure window, click the Hardware tab. In the Vendor Driver field, enter the name of the driver according to Table 1.
    Note: The Vendor driver file name is case sensitive. Enter only one driver name.
    Note: Change all driver file names from *.so to *.so.signed, if you upgrade a SNx device to Release 11.0.2 and later with the KNX VND integration already installed.
    Table 1. Vendor driver file name to use

    Network engine

    First driver

    Second driver

    NCE25, NAE35, NAE45, NAE55, NIE59

    libKNXDriver.so

    -
    SNExxxxx, SNCxxxxx libKNXDriver.so.signed -

    NAE85, OAS

    KNXDriver.dll

    KNXDriver_1.dll

    Figure 1. Insert Integration Wizard - configure

    Note: Do not modify the Vendor Reference field; it is not used in this integration.
  8. Click Next.
  9. In the Summary window, click Finish.