Requirements - Metasys - LIT-12013148 - System Integration - KNX Vendor Integration - 12.0

Network Engine Commissioning for KNX Vendor Integration Application Note

Brand
Metasys
Product name
KNX Vendor Integration
Document type
Application Note
Document number
LIT-12013148
Version
12.0
Revision date
2022-05-20
Language
English

To add a KNX integration as a VND integration, you must have the following:

  • A properly configured KNX system to communicate with KNX IP interfaces and KNX IP routers. All KNX line devices must be properly installed and communicating with KNX IP devices (interfaces and routers) before you add the integration in the Metasys Site Management Portal (SMP).
  • The KNX IP interfaces and KNX IP routers connected correctly to the network engine.