About this task
To insert a VND integration, complete the following steps:
Procedure
- Use the Launcher to log on to the network engine's SMP. If you need to install the Launcher, refer to the Launcher Installation Instructions (LIT-12011783).
- Drag the network engine device object from the navigation panel to the display panel. The Focus tab screen appears.
- Click Insert > Integration . The Insert Integration wizard appears.
- In the Select Object Type window, click VND Integration, and then click Next.
- In the Destination window, click the network engine object, and then click Next.
- In the Identifier window, enter a unique name for the integration trunk, and click Next.
-
In the Configure window,
click the Hardware tab. In the
Vendor Driver field, enter the name of the driver
according to Table 1.
Note: The Vendor driver file name is case sensitive. Enter only one driver name.
Table 1. Vendor driver file name to use Network engine
First driver
Second driver
NCE25, NAE35, NAE45, NAE55, NIE29, NIE39, NIE49, NIE59, SNExxxxx, SNCxxxxx
libKNXDriver.so
- NAE85
KNXDriver.dll
KNXDriver_1.dll
Figure 1. Insert Integration Wizard - configure
Note: Do not modify the Vendor Reference field; it is not used in this integration. - Click Next.
- In the Summary window, click Finish.