To add a KNX integration as a VND integration, you must have the following:
- A properly configured KNX system to communicate with KNX IP interfaces and KNX IP routers. All KNX line devices must be properly installed and communicating with KNX IP devices (interfaces and routers) before you add the integration in the Metasys Site Management Portal (SMP).
- The KNX IP interfaces and KNX IP routers connected correctly to the network engine.