Multistate Output - Metasys - LIT-12011924 - Supervisory Device - Network Engine - 9.0

NIEx9 Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Network Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12011924
Version
9.0
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Multistate Output

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

NUMBER_OF_STATES

X

   

74

 

X

2–5001

OBJECT_NAME

X

   

77

 

X

 

OUT_OF_SERVICE

X

   

81

 

X

 

PRESENT_VALUE

X

   

85

 

X

 

RELINQUISH_DEFAULT

X

   

104

 

X

 

ACKED_TRANSITIONS

 

X2

 

0

     

DESCRIPTION

 

X

 

28

 

X

64 characters max

DEVICE_TYPE

 

X

 

31

 

X

20 characters max

EVENT_ENABLE

 

X2

 

35

 

X

 

EVENT_MESSAGE_TEXTS

 

X2

 

351

     

EVENT_TIME_STAMPS

 

X2

 

130

     

FEEDBACK_VALUE

 

X2

 

40

 

X

 

NOTIFICATION_CLASS

 

X2

 

17

 

X

1–4, 194,303

NOTIFY_TYPE

 

X2

 

72

 

X

 

RELIABILITY

 

X

 

103

 

X3

 

STATE_TEXT

 

X

 

110

     

TIME_DELAY

 

X2

 

113

 

X

0–65,535

ALARM_MESSAGE_TEXT

   

X2

536

CharacterString

X

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZATION_CATEGORY

   

X

908

Enumerated

X

0–249

AUTO_RESTORE

   

X

561

Boolean

X

 

ENABLE_INTRINSIC_ALM

   

X

569

Boolean

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X2

32581

CharacterString

X

 

GRAPHIC_ALIAS

   

X2

32623

CharacterString

X

 

HEAVY_EQUIP_DELAY

   

X

516

Unsigned

X

 

HED_CONTROLLER

   

X

517

Unsigned

X

 

IGNORE_RELINQUISH_DEFAULT

   

X

580

Boolean

X

 

ITEM_REFERENCE

   

X

32527

CharacterString

   

LOCAL_CONTROL

   

X

32608

Boolean

X

 

NET_N2_ADDRESS

   

X

806

Unsigned

   

NET_POINT_TYPE

   

X

807

Enumerated

   

NET_POINT_ADDR

   

X

808

Unsigned

   

OFFLINE

   

X

913

Boolean

   

OVERRIDDEN

   

X

809

Boolean

   

REMOTE_DESCRIPTION

   

X4

32519

CharacterString

X

 

REMOTE_DEVICE_ADDR

   

X4

538

Complex

   

REMOTE_OBJECT_NAME

   

X4

2564

CharacterString

   

RESTORE_COMMAND_PRIORITY

   

X

721

Bit String

X

 

STATES_TEXT

   

X

931

Enumerated

X

 

STATUS

   

X

512

Enumerated

   

TRUNK_NUMBER

   

X

549

Unsigned

   

USER_NAME

   

X

2390

CharacterString

X

400 characters max

1 For N2 integrations, the range is 2–16.
2 Only present when intrinsic alarming is enabled.
3 Only writable when Out of Service is set to True.
4 Not present in all instances.