File - Metasys - LIT-12011924 - Supervisory Device - Network Engine - 9.0

NIEx9 Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Network Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12011924
Version
9.0
Language
English

File objects:

  • can be modified by replacing the entire file
  • must be written sequentially
  • are only visible during a backup or restore operation
  • can be created dynamically when restore is in progress

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. File

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

ARCHIVE

X

    13  

X

 

FILE_SIZE

X

    42  

X1

 

OBJECT_NAME

X

   

77

 

X

 

DESCRIPTION

 

X

 

28

 

X

64 characters max

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZATION_CATEGORY

   

X

908

Enumerated

X

0–249

CREATION_DATE

   

X

3381

Complex

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_PRIORITY

   

X

2197

Enumerated

X

0–3

ITEM_REFERENCE

   

X

32527

CharacterString

   

MAX_FILE_SIZE

   

X

3380

Unsigned

   

STATUS

   

X

512

Enumerated

   

USER_NAME

   

X

2390

CharacterString

X

400 characters max

1 Can write zero (0) to file size but arbitrary truncation or expansion is not supported.