Binary Value - Metasys - LIT-12011924 - Supervisory Device - Network Engine - 9.0

NIEx9 Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Network Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12011924
Version
9.0
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Binary Value

Property Name

Required

Optional

Proprie-tary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

PRESENT_VALUE

X

   

85

 

X

 

ACKED_TRANSITIONS

 

X1

 

0

     

ACTIVE_TEXT

 

X

 

4

 

X2

20 characters max

ACTIVE_TIME_RESET

 

X3

 

114

     

ALARM_VALUES

 

X1

 

7

 

X

 

COS_COUNT

 

X3

 

15

 

X

 

COS_TIME

 

X3

 

16

     

DESCRIPTION

 

X

 

28

 

X

64 characters max

ELAPSED_ACTIVE_TIME

 

X3

 

33

 

X

 

EVENT_ENABLE

 

X1

 

35

 

X

 

EVENT_MESSAGE_TEXTS

 

X1

  351      

EVENT_TIME_STAMPS

 

X1

 

130

     

INACTIVE_TEXT

 

X

 

46

 

X2

20 characters max

MIN_OFF_TIME

 

X3

 

66

 

X

0–4,294, 967,295

MIN_ON_TIME

 

X3

 

67

 

X

0–4,294, 967,295

NOTIFICATION_CLASS

 

X1

 

17

 

X

1–4, 194,303

NOTIFY_TYPE

 

X1

 

72

 

X

 

PRIORITY_ARRAY

 

X3

  87      

RELIABILITY

 

X

 

103

 

X

 

RELINQUISH_DEFAULT

 

X3

 

104

 

X

 

STATE_COUNT_RESET

 

X3

 

115

     

TIME_DELAY

 

X1

  113  

X

0–65,535

ALARM_MESSAGE_TEXT

   

X1

536

CharacterString

X

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZATION_CATEGORY

   

X

908

Enumerated

X

0–249

COV_COUNT

   

X3

839

Unsigned

   

DEVICE_MAC_ADDRESS

   

X3

3629

Unsigned

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X1

32581

CharacterString

X

 

GRAPHIC_ALIAS

   

X1

32623

CharacterString

X

 

IN_TEST

   

X3

3368

Boolean

   

INSTANCE_NUMBER

   

X

32589

Unsigned

   

INTRINSIC_ALARMING_DEFINED

   

X3

569

Boolean

X

 

ITEM_REFERENCE

   

X

32527

CharacterString

   

OFFLINE

   

X

913

Boolean

   

REMOTE_DESCRIPTION

   

X3

32519

CharacterString

X

 

REMOTE_DEVICE_ADDR

   

X3

538

Complex

   

REMOTE_OBJECT_NAME

   

X3

2564

CharacterString

   

RESTORE_COMMAND_PRIORITY

   

X

721

Bit String

X

 

STATES_TEXT

   

X

931

Enumerated

   

STATUS

   

X

512

Enumerated

   

TRUNK_NUMBER

   

X3

549

Unsigned

   

USER_NAME

   

X

2390

CharacterString

X

400 characters max

1 Only present when intrinsic alarm is enabled.
2 Not writable in all instances.
3 Not present in all instances.