Analog Value - Metasys - LIT-12011924 - Supervisory Device - Network Engine - 9.0

NIEx9 Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Network Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12011924
Version
9.0
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Analog Value

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

PRESENT_VALUE

X

    85  

X

 

UNITS

X

   

117

 

X

0–65,535

ACKED_TRANSITIONS

 

X1

 

0

     

COV_INCREMENT

 

X

 

22

 

X2

any value > 0

DEADBAND

 

X1

 

25

 

X

 

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ENABLE

 

X1

 

35

 

X

 

EVENT_MESSAGE_TEXTS

 

X1

  351      

EVENT_TIME_STAMPS

 

X1

 

130

     

HIGH_LIMIT

 

X1

 

45

 

X

 

LIMIT_ENABLE

 

X1

 

52

 

X

 

LOW_LIMIT

 

X1

 

59

 

X

 

NOTIFICATION_CLASS

 

X1

 

17

 

X

1–4, 194,303

NOTIFY_TYPE

 

X1

 

72

 

X

 

PRIORITY_ARRAY

 

X1

 

87

     

RELIABILITY

 

X

 

103

 

X

 

RELINQUISH_DEFAULT

 

X3

 

104

 

X

 

TIME_DELAY

 

X3

 

113

 

X

0–65,535

ALARM_MESSAGE_TEXT

   

X1

536

CharacterString

X

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZATION_CATEGORY

   

X

908

Enumerated

X

0–249

COV_COUNT

   

X3

839

Unsigned

   

DEVICE_MAC_ADDRESS

   

X3

3629

Unsigned

   

DISPLAY_PRECISION

   

X

661

Enumerated

X

0–12

ENABLED

   

X

673

Boolean

X

 

EXECUTION_PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X1

32581

CharacterString

X

 

GRAPHIC_ALIAS

   

X1

32623

CharacterString

X

 

IN_TEST

   

X

3368

Boolean

   

INSTANCE_NUMBER

   

X3

32589

Unsigned

   

INTRINSIC_ALARMING_DEFINED

   

X3

569

Boolean

X

 

ITEM_REFERENCE

   

X

32527

CharacterString

   

MAX_PRES_VALUE

   

X

65

Real

X4

 

MIN_PRES_VALUE

   

X

69

Real

X4

 

OFFLINE

   

X

913

Boolean

   

REMOTE_DESCRIPTION

   

X3

32519

CharacterString

X

 

REMOTE_DEVICE_ADDR

   

X3

538

Complex

   

REMOTE_OBJECT_NAME

   

X3

2564

CharacterString

   

RESTORE_COMMAND_PRIORITY

   

X

721

Bit String

X

 

STATUS

   

X

512

Enumerated

   

TRUNK_NUMBER

   

X3

549

Unsigned

   

USE_COV_MIN_SEND_ TIME

   

X3

3930

Boolean

X

 

USER_NAME

   

X

2390

CharacterString

X

400 characters max

1 Only present when intrinsic alarming is enabled.
2 Not writable in all instances.
3 Not present in all instances.
4 For NCE, only writable for AVs on supervisory side, not on field controller side.