Network Security Options - Metasys - LIT-12011924 - Supervisory Device - Network Engine - 9.0

NIEx9 Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Network Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12011924
Version
9.0
Language
English

Non-secure Device - is capable of operating without BACnet Network Security

Secure Device - is capable of using BACnet Network Security (NS-SD BIBB)

 

Multiple Application-Specific Keys

 

Supports encryption (NS-ED BIBB)

 

Key Server (NS-KS BIBB)