Character Sets Supported - Metasys - LIT-12011924 - Supervisory Device - Network Engine - 9.0

NIEx9 Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Network Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12011924
Version
9.0
Language
English

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

ISO 10646 Unicode Transformation Format-8 (UTF-8)

   

IBM/Microsoft® Double-Byte Character Set (DBCS)

   

ISO 8859-1

ISO 10646 Universal Character Set-2 (UCS-2)

   

ISO 10646 (UCS-4)

   

Japanese Industrial Standard (JIS) X 0208