Product Description - Metasys - LIT-12011924 - Supervisory Device - Network Engine - 9.0

NIEx9 Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Network Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12011924
Version
9.0
Language
English

The NIEx9 is a component of the Metasys® system. In terms of the BACnet protocol, the NIEx9 is a building controller and supports many operator workstation services.

The NIEx9 can monitor and supervise a network of BACnet and non BACnet devices. An operator views the data on a web browser that is logged on to the web-enabled user interface of a NIEx9. As a building controller, other BACnet devices on the network can read and write to the BACnet objects within a NIEx9.