Dual Trunk Integration - Metasys - LIT-12011919 - MS-KNXN89-0 - MS-MBUSN89-0 - MS-MODBUSN89-0 - MS-NIE2910-0 - MS-NIE2916-0 - MS-NIE2920-0 - MS-NIE2926-0 - MS-NIE2960-0 - MS-NIE2966-0 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE4910-2 - MS-NIE4920-2 - MS-NIE5920-2 - MS-NIE5960-2 - MS-NIE89SW-0 - MS-NIE89SW-6 - Bulb controller - NIEx9 Network Integration Engine - 7

NIEx9 Driver Manager Application Note

Product
Network Engines > Network Control Engines > NIEx9 Network Integration Engine
Document type
Application Note
Document number
LIT-12011919
Version
7
Revision date
01/08/2017

Starting at Metasys system Release 7.0, dual trunk integration support is available as a factory standard on NIE29, NIE39, NIE49, and NIE59 models shipped with the date code of RY10416 or later. For NIEx9s purchased prior to this release, you can apply the dual trunk integration feature using the NIEx9 Driver Manager tool. For information on how to apply the dual trunk functionality to older NIEx9s, see Updating the NIE DLL Protocol.