Introduction - Metasys - LIT-12011919 - MS-MBUSN89-0 - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - NIEx9 Network Integration Engine - 7

NIEx9 Driver Manager Application Note

Product
Network Engines > Network Control Engines > NIEx9 Network Integration Engine
Document number
LIT-12011919
Version
7
Revision date
2017-08-01

The NIEx9 Driver Manager tool allows you to upload driver and license files related to the Network Integration Engine (NIE) for third-party integration solutions.

This tool also allows you to perform the following tasks:

  • manage the backup and restoration of NIEx9 files before device reformatting with the NAE/NIE Update Tool
  • save files to a working directory on your local computer
  • upload files back to the NIE when a new device image is updated
  • upgrade the Vendor protocol DLL as enhancements or bug fixes are released