Detailed Procedures - Metasys - LIT-12011919 - MS-MBUSN89-0 - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - NIEx9 Network Integration Engine - 7

NIEx9 Driver Manager Application Note

Product
Network Engines > Network Control Engines > NIEx9 Network Integration Engine
Document number
LIT-12011919
Version
7
Revision date
2017-08-01

Use the Driver Manager tool to:

  • specify application settings
  • connect to the NIEx9
  • upload the license file
  • download the license file
  • upload a solution
  • download a solution
  • upload Modbus tables
  • update the NIE DLL protocol
  • display tool information
  • connect to the NIE with a Remote Desktop
  • install the NIE59 FTP server
  • verify the NIE59 FTP server

The following sections describe each operation.