Uploading Solutions - Metasys - LIT-12011919 - MS-MBUSN89-0 - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - NIEx9 Network Integration Engine - 7

NIEx9 Driver Manager Application Note

Product
Network Engines > Network Control Engines > NIEx9 Network Integration Engine
Document number
LIT-12011919
Version
7
Revision date
2017-08-01

Procedure

  1. Click the Upload Solutions tab (Figure 1).
  2. Select the solutions you want to upload in the Select row column.
  3. Click Upload. The uploaded solution package (.SIS) is placed in the working folder.
    Figure 1. Upload Solutions Tab

    Table 1. Upload Solutions Tab Descriptions

    Name

    Description

    Solutions Table

    Lists all the solutions that are on the NIEx9.

    You can select one or more to perform the upload.

    Disconnect

    Disconnects the Driver Manager from the NIEx9.

    Note: Clicking Disconnect does not exit the NIEx9 Driver Manager application.

    Upload

    Uploads the solution packages the NIEx9 and saves the packages to the working folder.

    Connect UI

    Connects to the Metasys user interface.

    Connect FTP

    Connects to the FTP server in an NIE29, 39, or 49.

    Note: For an NIE59, you can connect to the FTP server only when the Filezilla FTP client is installed on your computer.