Downloading the License File - Metasys - LIT-12011919 - MS-MBUSN89-0 - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - NIEx9 Network Integration Engine - 7

NIEx9 Driver Manager Application Note

Product
Network Engines > Network Control Engines > NIEx9 Network Integration Engine
Document type
Application Note
Document number
LIT-12011919
Version
7
Revision date
01/08/2017

Procedure

  1. Click the Download License tab.

    The MAC Address is automatically populated.

  2. Select the type of integration that is authorized for the NIEx9.
  3. Click Download.
    The license file is downloaded directly to the connected NIEx9.
    Figure 1. Download License Tab

    Table 1. Download License Tab Descriptions

    Name

    Description

    MAC Address

    The MAC address of the connected NIEx9.

    Type

    Indicates the type of license that must be downloaded: Generic, OPC Server Integration, or ISN Integration

    OPC Server and ISN are custom solutions. For additional details, contact the Johnson Controls Field Support Center.

    Disconnect

    Disconnects the Driver Manager from the NIEx9.

    Clicking Disconnect does not exit the NIEx9 Driver Manager application.

    Download

    Downloads the license to the connected NIEx9. The license file must be in the selected working folder.

    Connect UI

    Connects to the Metasys user interface.

    Connect FTP

    Connects to the FTP server in an NIE29, 39, or 49.

    Note: For an NIE59, you can connect to the FTP server only when the Filezilla FTP client is installed on your computer.