Downloading Solutions - Metasys - LIT-12011919 - MS-KNXN89-0 - MS-MBUSN89-0 - MS-MODBUSN89-0 - MS-NIE2910-0 - MS-NIE2916-0 - MS-NIE2920-0 - MS-NIE2926-0 - MS-NIE2960-0 - MS-NIE2966-0 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE4910-2 - MS-NIE4920-2 - MS-NIE5920-2 - MS-NIE5960-2 - MS-NIE89SW-0 - MS-NIE89SW-6 - Bulb controller - NIEx9 Network Integration Engine - 7

NIEx9 Driver Manager Application Note

Product
Network Engines > Network Control Engines > NIEx9 Network Integration Engine
Document type
Application Note
Document number
LIT-12011919
Version
7
Revision date
01/08/2017

Procedure

  1. Click the Download Solutions tab.
  2. Select the solutions you want to download in the Select row column.
  3. Click Download.
    The selected solutions are downloaded into the connected NIEx9.
    Figure 1. Download Solutions Tab

    Table 1. Download Solution Tab Descriptions

    Name

    Description

    Solutions Table

    Lists all the solutions that are in the default packages folder and in the selected working folder.

    The white rows are the solutions (packages) that are present in the default directory.

    The green rows are the solutions uploaded from the NIE device and stored in the working directory.

    You can select one or more to perform the download.

    Disconnect

    Disconnects from the NIEx9 to which the Driver Manager is currently connected.

    Clicking Disconnect does not exit the NIEx9 Driver Manager application.

    Download

    Downloads the selected packages to the connected NIEx9.

    Connect UI

    Connects to the Metasys user interface.

    Connect FTP

    Connects to the FTP server in an NIE29, 39, or 49.

    Note: For an NIE59, you can connect to the FTP server only when the Filezilla FTP client is installed on your computer.