Displaying Tool Information - Metasys - LIT-12011919 - MS-MBUSN89-0 - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - NIEx9 Network Integration Engine - 7

NIEx9 Driver Manager Application Note

Product
Network Engines > Network Control Engines > NIEx9 Network Integration Engine
Document type
Application Note
Document number
LIT-12011919
Version
7
Revision date
01/08/2017

About this task

Click the About tab to view version and copyright information for the NIEx9 Driver Manager tool (Figure 1). To check for an updated version of the NIEx9 Driver Manager, click Check for Updates. If a newer version is available, clicking the button serves up a zip file of the NIEx9 Driver Manager that you can download to your computer for installation. If a newer version is not available, a dialog box appears to indicate that you have the latest software version.

Figure 1. About Tab