Conclusion - Metasys - LIT-12013296 - M4-SNC16120-0 - M4-SNC16120-04 - M4-SNC16121-0 - M4-SNC16121-04 - M4-SNC25150-0 - M4-SNC25150-04 - M4-SNC25151-0 - M4-SNC25151-04 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE10502-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE11002-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - M4-SNE22002-0 - Supervisory Device - M4-SNC Network Controller - M4-SNE Network Engine - NAE85 Network Automation Engine - 13.0

NAE85/M4-SNE/M4-SNC Product Bulletin

Product
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Product Bulletin
Document number
LIT-12013296
Version
13.0
Revision date
2024-08-26
Product status
Active

The SNE, SNC, and NAE85 affirm the position of Johnson Controls as a leader and innovator in the Building Automation System (BAS) industry. The integration of IT and Internet standards into the SNE and SNC platform, as well as the use of open protocols for field networks, bring the benefits of the global communications and control industries into one system. Web browser-based access from any location is a key to the effective use of the automation network.

The Metasys system continues to be the integrating network within buildings and has now been extended to bridge the gap between traditional control systems and the business and communication network systems of the enterprise.