|
Problem |
Solution |
|---|---|
|
You receive the following error message when installing an NAE85:
|
Metasys SCT is installed on the computer. Click OK, and uninstall SCT on the computer. When the SCT is uninstalled, follow Installing or upgrading an NAE85 steps to install the NAE85. |
|
The following message appears when you are logged in to an NAE85:
|
Complete one of the following steps:
|
|
You experience installation problems and would like to consult the error log. |
Error messages for installation problems are located here: C:\Users\<name_of_currently_logged_in_user>\AppData\Local It is called Metasys_Network_Engine_11.0_x.html, where x is a time/date stamp in the format YYYYMMDDHHMMSS. For example: Metasys_Network_Engine_11.0_20180831113343.html |
|
You experience problems when upgrading your NAE85. |
If the system is using the 9.0 iterations of the software, you must uninstall the software before you can upgrade an NAE85 to a more recent release. Follow these steps to resolve the issue:
|
|
During the upgrade procedure, the following error message appears and the progress bar does not advance:
|
The device manager service could not be deleted during the installation. Click OK to proceed with the installation. If you click OK and the upgrade does not progress, continue with these steps:
|