Trend Log Multiple - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Trend Log Multiple

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

ENABLE

X

   

133

 

X

 

OBJECT_NAME

X

   

77

 

X

 

PROPERTY_ LIST

X

   

371

     

STOP_WHEN_ FULL

X

   

144

 

X

 

ACKED_ TRANSITIONS

 

X1

  0      

CLIENT_COV_ INCREMENT

 

X

  127  

X

 

COV_RESUBSC_ INTERVAL

 

X

 

128

 

X

Any value > 0

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X1

 

35

 

X2

 

EVENT_ MESSAGE_ TEXTS

 

X1

 

351

     
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X2 256 characters max

EVENT_TIME_ STAMPS

 

X1

 

130

     

LOG_INTERVAL

 

X3

 

134

 

X

 

LOGGING_ DEVICE

 

X

  183      

LOGGING_TYPE

 

X

 

197

     

NOTIFICATION _CLASS

 

X1

 

17

 

X2

1–4,194,303

NOTIFY_ THRESHOLD

 

X1

 

137

 

X2

 

NOTIFY_TYPE

 

X1

 

72

 

X2

 

RECORD_ COUNT

 

X

 

141

 

X

 

RECORDS_ SINCE_ NOTIFICATION

 

X1

 

140

     

START_TIME

 

X

 

142

 

X

 

STOP_TIME

 

X

 

143

 

X

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

BUFFER_STATE

   

X

2565

Enumerated

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

INPUT_REF

   

X

545

Complex

   

INTRINSIC_ ALARMING_ DEFINED

   

X

569

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

NEXT_ TRANSFER_ COUNT

   

X

2553

Unsigned

   

REMOTE_ DESCRIPTION

   

X4

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X4

538

Complex

   

REMOTE_ OBJECT_NAME

   

X4

2564

Character String

   

RESPOSITORY_ ENABLED

   

X

2549

Boolean

X

 

ROUTE_ TRIGGER

   

X

2552

Boolean

X

 

SAMPLE_ INTERVAL

   

X3

2566

Unsigned

X

 

STATUS

   

X

512

Enumerated

   

TRANSFER_ SETPOINT

   

X

2550

Unsigned

X

1–5,000

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Only present when intrinsic alarming is enabled.
2 Only writable when intrinsic alarming is enabled.
3 Log_Interval and Sample_Interval represent the same value in different units of time. Log_Interval is in hundredths of seconds and Sample_Interval (JCI proprietary) is in seconds. Both allow only whole seconds and round to the nearest second.
4 Not present in all instances.