Trend Log - Metasys - LIT-1201532 - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE85 Network Automation Engine - NAE45 Network Automation Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Document number
LIT-1201532
Version
9
Revision date
2019-04-09

Dynamically Creatable: Yes

Dynamically Deletable: Yes

Table 1. Trend Log

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

BUFFER_SIZE

X

   

126

 

X1

2-5000

ENABLE

X

   

133

 

X

 

LOGGING_ TYPE

X

    197  

X1

 

OBJECT_NAME

X

    77  

X

 

PROPERTY_ LIST

X

   

371

     

STOP_WHEN_ FULL

X

   

144

 

X

 

ACKED_ TRANSITION

 

X2

 

0

     

CLIENT_COV_ INCREMENT

 

X

 

127

 

X

 

COV_RESUBSC_ INTERVAL

 

X

 

128

 

X

Any value > 0

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X2

 

35

 

X3

 

EVENT_ MESSAGE_ TEXTS

 

X2

 

351

     
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X3 256 characters max

EVENT_TIME_ STAMPS

 

X2

 

130

     

INPUT_ REFERENCE 4

 

X

 

132

 

X1

 

LOG_INTERVAL

 

X5

 

134

 

X

 

LOGGING_ TYPE

 

X

  197  

X1

 

NOTIFICATION _CLASS

 

X2

 

17

 

X3

1–4,194,303

NOTIFY_ THRESHOLD

 

X2

 

137

 

X3

 

NOTIFY_TYPE

 

X2

 

72

 

X3

 

RECORD_ COUNT

 

X

 

141

 

X

 

RECORDS_ SINCE_ NOTIFICATION

 

X2

 

140

     

RELIABILITY

 

X

 

103

     

START_TIME

 

X

 

142

 

X

 

STOP_TIME

 

X

 

143

 

X

 

TRIGGER

 

X

 

205

 

X

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

BUFFER_STATE

   

X

2565

Enumerated

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

INPUT_REF

   

X

545

Complex

   

INTRINSIC_ ALARMING_ DEFINED

   

X6

569

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

NEXT_ TRANSFER_ COUNT

   

X

2553

Unsigned

   

REMOTE_ DESCRIPTION

   

X6

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X6

538

Complex

   

REMOTE_ OBJECT_NAME

   

X6

2564

Character String

   

RESPOSITORY_ ENABLED

   

X

2549

Boolean

X

 

ROUTE_ TRIGGER

   

X

2552

Boolean

X

 

SAMPLE_ INTERVAL

   

X5

2566

Unsigned

X

 

STATUS

   

X

512

Enumerated

   

TRANSFER_ SETPOINT

   

X

2550

Unsigned

X

1–5,000

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Not writable in all instances.
2 Only present when intrinsic alarming is enabled.
3 Only writable when intrinsic alarming is enabled.
4 Named LOG_DEVICEOBJECTPROPERTY in the BACnet standard.
5 Log_Interval and Sample_Interval represent the same value in different units of time. Log_Interval is in hundredths of seconds and Sample_Interval (Johnson Controls proprietary) is in seconds. Both allow only whole seconds and round to the nearest second.
6 Not present in all instances.