Pulse Converter - Metasys - LIT-1201532 - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE85 Network Automation Engine - NAE45 Network Automation Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Document number
LIT-1201532
Version
9
Revision date
2019-04-09

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Pulse Converter

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

OUT_OF_ SERVICE

X

   

81

 

X

 

PRESENT_ VALUE

X

   

85

 

X

 

PROPERTY_ LIST

X

   

371

     

UNITS

X

    117  

X

0–65,535

ACKED_ TRANSITIONS

 

X1

 

0

     

DEADBAND

 

X

 

25

 

X

 

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X1

 

35

 

X2

 

EVENT_ MESSAGE_ TEXTS

 

X1

 

351

     
EVENT_ MESSAGE_ TEXTS_CONFIG   X   352   X2 256 characters max

EVENT_STATE

 

X

 

36

     

EVENT_TIME_ STAMPS

 

X1

 

130

     

HIGH_LIMIT

 

X1

 

45

 

X2

 

LIMIT_ENABLE

 

X1

 

52

 

X2

 

LOW_LIMIT

 

X1

 

59

 

X2

 

NOTIFICATION _CLASS

 

X1

 

17

 

X2

1–4,194,303

NOTIFY_TYPE

 

X1

 

72

 

X2

 

PULSE_ REFERENCE

 

X

 

181

     

RELIABILITY

 

X

 

103

 

X3

 

TIME_DELAY

 

X1

 

113

 

X2

0–65,535

ALARM_ MESSAGE_ TEXT

   

X1

536

Character String

X2

 

COUNT BEFORE DECREMENT

   

X

3629

Unsigned

   

COUNT CHANGE TIME

   

X

549

Unsigned

   

DECREMENT PRESENT VALUE

   

X

2197

Enumerated

X

0–3

DISPLAY_ PRECISION

   

X

661

Enumerated

X

 

GRAPHIC

   

X1

32581

Character String

X2

 

GRAPHIC_ ALIAS

   

X1

32623

Character String

X2

 

INITIAL_READ_ DONE

   

X

64585

Boolean

   

INPUT REF

   

X

512

Enumerated

   

INSTANCE_ NUMBER

    X

32589

Unsigned

   

INTRINSIC_ ALARMING_ DEFINED

   

X4

569

Boolean

X

 

OFFLINE

   

X

913

Boolean

   

PULSE COUNT

   

X

1006

Enumerated

   

PULSE SCALE FACTOR

   

X

673

Boolean

X

 

REMOTE_ DESCRIPTION

   

X4

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X4

538

Complex

   

REMOTE_ OBJECT_NAME

   

X4

2564

Character String

   

STATUS

   

X

512

Enumerated

   

UPDATE TIME

   

X

32589

Unsigned

   
1 Only present when intrinsic alarming is enabled.
2 Only writable when intrinsic alarming is enabled.
3 Only writable when Out of Service is set to True.
4 Not present in all instances.