Positive Integer Value - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Positive Integer Value

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

PRESENT_ VALUE

X

    85  

X

 

PROPERTY_ LIST

X

   

371

     

UNITS

X

   

117

 

X

0–65,535

ACKED_ TRANSITIONS

 

X1

 

0

     

COV_ INCREMENT

 

X

 

22

 

X

any value > 0

DEADBAND

 

X1

 

25

 

X2

 

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X1

 

35

 

X2

 

EVENT_ MESSAGE_ TEXTS

 

X1

 

351

     
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X2 256 characters max

EVENT_STATE

 

X1

 

36

     

EVENT_TIME_ STAMPS

 

X1

 

130

     

HIGH_LIMIT

 

X1

  45  

X2

 

LIMIT_ENABLE

 

X1

 

52

 

X2

 

LOW_LIMIT

 

X1

 

59

 

X2

 

MAX_PRES_ VALUE

 

X

 

65

 

X

 

MIN_PRES_ VALUE

 

X

 

69

 

X

 

NOTIFICATION _CLASS

 

X1

 

17

 

X2

1–4,194,303

NOTIFY_TYPE

 

X1

  72  

X2

 

OUT_OF_ SERVICE

 

X

 

81

 

X

 

PRIORITY_ ARRAY

 

X

 

87

     

PROFILE_ NAME

 

X

 

168

     

RELIABILITY

 

X

 

103

 

X

 

RELINQUISH_ DEFAULT

 

X

 

104

     

TIME_DELAY

 

X1

 

113

 

X2

0–65,535

ALARM_ MESSAGE_ TEXT

   

X1

536

Character String

X2

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X1

32581

Character String

X2

 

GRAPHIC_ ALIAS

   

X1

32623

Character String

X2

 

INSTANCE_ NUMBER

   

X

32589

Unsigned

   

INTRINSIC_ ALARMING_ DEFINED

   

X3

569

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

REMOTE_ DESCRIPTION

   

X3

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X3

538

Complex

   

REMOTE_ OBJECT_NAME

   

X3

2564

Character String

   

STATUS

   

X

512

Enumerated

   
1 Only present when intrinsic alarming is enabled.
2 Only writable when intrinsic alarming is enabled.
3 Not present in all instances.