Multistate Output - Metasys - LIT-1201532 - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE85 Network Automation Engine - NAE45 Network Automation Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Document number
LIT-1201532
Version
9
Revision date
2019-04-09

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Multistate Output

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

NUMBER_ OF_STATES

X

   

74

 

X

2–500 1

OBJECT_NAME

X

   

77

 

X

 

OUT_OF_ SERVICE

X

   

81

 

X

 

PRESENT_ VALUE

X

   

85

 

X

 

PROPERTY_ LIST

X

   

371

     

RELINQUISH_ DEFAULT

X

   

104

 

X

 

ACKED_ TRANSITIONS

 

X2

 

0

     

DESCRIPTION

 

X

 

28

 

X

64 characters max

DEVICE_TYPE

 

X

 

31

 

X

20 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ ENABLE

 

X2

 

35

 

X3

 

EVENT_ MESSAGE_ TEXTS

 

X2

 

351

     
EVENT_ MESSAGE_ TEXTS_CONFIG   X   352   X 256 characters max

EVENT_TIME_ STAMPS

 

X2

 

130

     

FEEDBACK_ VALUE

 

X2

 

40

 

X3

 

NOTIFICATION _CLASS

 

X2

 

17

 

X3

1–4,194,303

NOTIFY_TYPE

 

X2

 

72

 

X3

 

RELIABILITY

 

X

 

103

 

X4

 

STATE_TEXT

 

X

 

110

     

TIME_DELAY

 

X2

 

113

 

X3

0–65,535

ALARM_ MESSAGE_ TEXT

   

X2

536

Character String

X3

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

AUTO_ RESTORE

   

X

561

Boolean

X

 

ENABLE_ INTRINSIC_ ALM

   

X

569

Boolean

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X2

32581

Character String

X3

 

GRAPHIC_ ALIAS

   

X2

32623

Character String

X3

 

HEAVY_EQUIP_ DELAY

   

X

516

Unsigned

X

 

HED_ CONTROLLER

   

X

517

Unsigned

X

 

IGNORE_ RELINQUISH_ DEFAULT

   

X

580

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

LOCAL_ CONTROL

   

X

32608

Boolean

X

 

NET_N2_ ADDRESS

   

X

806

Unsigned

   

NET_POINT_ TYPE

   

X

807

Enumerated

   

NET_POINT_ ADDR

   

X

808

Unsigned

   

OFFLINE

   

X

913

Boolean

   

OVERRIDDEN

   

X

809

Boolean

   

REMOTE_ DESCRIPTION

   

X5

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X5

538

Complex

   

REMOTE_ OBJECT_NAME

   

X5

2564

Character String

   

RESTORE_ COMMAND_ PRIORITY

   

X

721

Bit String

X

 

STATES_TEXT

   

X

931

Enumerated

X

 

STATUS

   

X

512

Enumerated

   

TRUNK_ NUMBER

   

X

549

Unsigned

   

USER_NAME

   

X

2390

Character String

X

400 characters max

1 For N2 integrations, the range is 2–16.
2 Only present when intrinsic alarming is enabled.
3 Only writable when intrinsic alarming is enabled.
4 Only writable when Out of Service is set to True.
5 Not present in all instances.