Multistate Input - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Multistate Input

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

NUMBER_OF_ STATES

X

   

74

 

X

2–500 1

OBJECT_NAME

X

   

77

 

X

 

OUT_OF_ SERVICE

X

    81  

X

 

PRESENT_ VALUE

X2

    85  

X

 

PROPERTY_ LIST

X

   

371

     

ACKED_ TRANSITIONS

 

X3

 

0

     

ALARM_ VALUES

 

X3

 

7

 

X4

0–65,535

DESCRIPTION

 

X

 

28

 

X

64 characters max

DEVICE_TYPE

 

X

 

31

 

X

20 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X3

 

35

 

X4

 
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X4 256 characters max

EVENT_TIME_ STAMPS

 

X3

 

130

     

FAULT_VALUES

 

X3

 

39

 

X4

0–65,535

NOTIFICATION _CLASS

 

X3

 

17

 

X4

1–4,194,303

NOTIFY_TYPE

 

X3

 

72

 

X4

 

RELIABILITY

 

X

 

103

 

X2

 

STATE_TEXT

 

X

 

110

     

TIME_DELAY

 

X3

 

113

 

X4

0–65,535

ALARM_ MESSAGE_ TEXT

   

X3

536

Character String

X4

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

ENABLE_ INTRINSIC_ ALM

   

X

569

Boolean

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X3

32581

Character String

X4

 

GRAPHIC_ ALIAS

   

X3

32623

Character String

X4

 

ITEM_ REFERENCE

   

X

32527

Character String

   

NET_N2_ ADDRESS

   

X

806

Unsigned

   

NET_POINT_ ADDR

   

X

808

Unsigned

   

NET_POINT_ TYPE

   

X

807

Enumerated

   

OFFLINE

   

X

913

Boolean

   

OVERRIDDEN

   

X

809

Boolean

   

REMOTE_ DESCRIPTION

   

X5

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X5

538

Complex

   

REMOTE_ OBJECT_NAME

   

X5

2564

Character String

   

STATES_TEXT

   

X

931

Enumerated

X

 

STATUS

   

X

512

Enumerated

   

TRUNK_ NUMBER

   

X

549

Unsigned

   

USER_NAME

   

X

2390

Character String

   
1 For N2 integrations, the range is 2-16.
2 Only writable when Out of Service is set to True.
3 Only present when intrinsic alarming is enabled.
4 Only writable when intrinsic alarming is enabled.
5 Not present in all instances.