Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
OBJECT_NAME |
X |
77 |
X |
||||
PRESENT_ VALUE |
X |
85 |
X |
||||
PROPERTY_ LIST |
X |
371 |
|||||
UNITS |
X |
117 |
X |
0–65,535 |
|||
ACKED_ TRANSITIONS |
X1 |
0 |
|||||
COV_ INCREMENT |
X |
22 |
X |
any value > 0 |
|||
DEADBAND |
X1 |
25 |
X2 |
||||
DESCRIPTION |
X |
28 |
X |
64 characters max |
|||
EVENT_ DETECTION_ ENABLE | X | 353 | |||||
EVENT_ENABLE |
X1 |
35 |
X2 |
||||
EVENT_ MESSAGE_ TEXTS |
X1 |
351 | |||||
EVENT_ MESSAGE_ TEXTS_ CONFIG | X | 352 | X2 | 256 characters max | |||
EVENT_STATE |
X1 |
36 |
|||||
EVENT_TIME_ STAMPS |
X1 |
130 |
|||||
HIGH_LIMIT |
X1 |
45 |
X2 |
||||
LIMIT_ENABLE |
X1 |
52 |
X2 |
||||
LOW_LIMIT |
X1 |
59 |
X2 |
||||
MAX_PRES_ VALUE |
X |
65 |
X |
||||
MIN_PRES_ VALUE |
X |
69 |
X |
||||
NOTIFICATION _CLASS |
X1 |
17 |
X2 |
1–4,194,303 |
|||
NOTIFY_TYPE |
X1 |
72 |
X2 |
||||
OUT_OF_ SERVICE |
X |
81 |
X |
||||
PRIORITY_ ARRAY |
X |
87 | |||||
PROFILE_ NAME |
X |
168 |
|||||
RELIABILITY |
X |
103 |
X |
||||
RELINQUISH_ DEFAULT |
X |
104 |
X |
||||
TIME_DELAY |
X1 |
113 |
X2 |
0–65,535 |
|||
ALARM_ MESSAGE_ TEXT |
X1 |
536 |
Character String |
X2 |
|||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
AUTHORIZA- TION_ CATEGORY |
X |
908 |
Enumerated |
X |
0–249 |
||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_ PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
GRAPHIC |
X1 |
32581 |
Character String |
X2 |
|||
GRAPHIC_ ALIAS |
X1 |
32623 |
Character String |
X2 |
|||
INSTANCE_ NUMBER |
X |
32589 |
Unsigned |
||||
INTRINSIC_ ALARMING_ DEFINED |
X3 |
569 |
Boolean |
X |
|||
ITEM_ REFERENCE |
X |
32527 |
Character String |
||||
REMOTE_ DESCRIPTION |
X |
32519 |
Character String |
X |
|||
REMOTE_ DEVICE_ADDR |
X3 |
538 |
Complex |
||||
REMOTE_ OBJECT_NAME |
X3 |
2564 |
Character String |
||||
STATUS |
X |
512 |
Enumerated |
||||
USER_NAME |
X |
2390 |
Character String |
X |
400 characters max |