File objects:
- can be modified by replacing the entire file
- must be written sequentially
- are only visible during a backup or restore operation
- can be created dynamically when restore is in progress
Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
ARCHIVE |
X |
13 |
X |
||||
FILE_SIZE |
X |
42 |
X1 |
||||
OBJECT_NAME |
X |
77 |
X |
||||
PROPERTY_ LIST |
X |
371 |
|||||
DESCRIPTION |
X |
28 |
X |
64 characters max |
|||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
AUTHORIZA- TION_ CATEGORY |
X |
908 |
Enumerated |
X |
0–249 |
||
CREATION_ DATE |
X |
3381 |
Complex |
||||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_ PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
ITEM_ REFERENCE |
X |
32527 |
Character String |
||||
MAX_FILE_SIZE |
X |
3380 |
Unsigned |
||||
STATUS |
X |
512 |
Enumerated |
||||
USER_NAME |
X |
2390 |
Character String |
X |
400 characters max |
1 Can write zero (0) to file size
but arbitrary truncation or expansion is not
supported.