Event Enrollment - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

Dynamically Creatable: Yes

Dynamically Deletable: Yes

Table 1. Event Enrollment

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

EVENT_ENABLE

X

   

35

 

X

 

EVENT_ PARAMETERS

X

   

83

 

X

 

NOTIFICATION _CLASS

X

   

17

 

X

1–4,194,303

NOTIFY_TYPE

X

   

72

 

X

 

OBJECT_NAME

X

    77  

X

 

OBJECT_ PROPERTY_ REFERENCE

X

   

78

 

X1

 

PROPERTY_ LIST

X

   

371

     

RELIABILITY

X2

   

103

     

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ DETECTION_ ENABLE  

X

  353      

EVENT_ MESSAGE_ TEXTS

 

X

 

351

     
EVENT_ MESSAGE_ TEXTS_CONFIG  

X

 

352

  X

256 characters max

ALARM_ DISABLED     X 4308 Boolean X  

ALARM_ MESSAGE_ TEXT

   

X

536

Character String

X

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X

32581

Character String

X

 

GRAPHIC_ ALIAS

   

X

32623

Character String

X

 

INPUT_REF

   

X

545

Complex

   

ITEM_ REFERENCE

   

X

32527

Character String

   

JCI_EVENT_ PARAMETERS

   

X

2571

Character String

X

 

REMOTE_ DESCRIPTION

   

X3

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X3

538

Complex

   

REMOTE_ OBJECT_NAME

   

X3

2564

Character String

   

STATUS

   

X

512

Enumerated

   
STORED_ EVENT_ ENABLE    

X

4306 Boolean X  

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Only writable when not defined after create object.
2 Only writable when intrinsic alarming is enabled.
3 Not present in all instances.