Character String Value - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Character String Value

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

PRESENT_ VALUE

X

   

85

 

X

 

PROPERTY_ LIST

X

   

371

     

ACKED_ TRANSITIONS

 

X1

 

0

     

ALARM_ VALUES

 

X1

  7  

X2

 

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X1

 

35

 

X2

 

EVENT_ MESSAGE_ TEXTS

 

X1

  351      
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X2 256 characters max

EVENT_STATE

 

X1

 

36

     

EVENT_TIME_ STAMPS

 

X1

 

130

     

FAULT_VALUES

 

X3

 

39

 

X

0–65,535

NOTIFICATION _CLASS

 

X1

 

17

 

X2

1–4,194,303

NOTIFY_TYPE

 

X1

 

72

 

X2

 

OUT_OF_ SERVICE

 

X

 

81

 

X

 

PRIORITY_ ARRAY

 

X3

 

87

     

PROFILE_NAME

 

X

 

168

     

RELIABILITY

 

X

  103  

X

 

RELINQUISH_ DEFAULT

 

X3

 

104

 

X

 

TIME_DELAY

 

X1

 

113

 

X2

0–65,535

ALARM_ MESSAGE_ TEXT

   

X1

536

Character String

X2

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X1

32581

Character String

X2

 

GRAPHIC_ ALIAS

   

X1

32623

Character String

X2

 

INSTANCE_ NUMBER

   

X

32589

Unsigned

   

INTRINSIC_ ALARMING_ DEFINED

   

X3

569

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

REMOTE_ DESCRIPTION

   

X3

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X3

538

Complex

   

REMOTE_ OBJECT_NAME

   

X3

2564

Character String

   

STATUS

   

X

512

Enumerated

   

STATUS FLAGS

   

X

512

Enumerated

   

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Only present when intrinsic alarming is enabled.
2 Only writable when intrinsic alarming is enabled.
3 Not present in all instances.