Binary Value - Metasys - LIT-1201532 - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE85 Network Automation Engine - NAE45 Network Automation Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Document number
LIT-1201532
Version
9
Revision date
2019-04-09

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Binary Value

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

PRESENT_ VALUE

X

   

85

 

X

 

PROPERTY_ LIST

X

   

371

     

ACKED_ TRANSITIONS

 

X1

 

0

     

ACTIVE_TEXT

 

X

 

4

 

X2

20 characters max

ACTIVE_TIME_ RESET

 

X3

 

114

     

ALARM_ VALUES

 

X1

 

7

 

X4

 

COS_COUNT

 

X3

 

15

 

X

 

COS_TIME

 

X3

 

16

     

DESCRIPTION

 

X

 

28

 

X

64 characters max

ELAPSED_ ACTIVE_ TIME

 

X3

 

33

 

X

 
EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X1

 

35

 

X4

 

EVENT_ MESSAGE_ TEXTS

 

X1

  351      
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X4 256 characters max

EVENT_TIME_ STAMPS

 

X1

 

130

     

INACTIVE_TEXT

 

X

 

46

 

X2

20 characters max

MIN_OFF_TIME

 

X3

 

66

 

X

0–4,294,967, 295

MIN_ON_TIME

 

X3

 

67

 

X

0–4,294,967, 295

NOTIFICATION _CLASS

 

X1

 

17

 

X4

1–4,194,303

NOTIFY_TYPE

 

X1

 

72

 

X4

 

PRIORITY_ ARRAY

 

X3

  87      

RELIABILITY

 

X

 

103

 

X

 

RELINQUISH_ DEFAULT

 

X3

 

104

 

X

 

STATE_COUNT _RESET

 

X3

 

115

     

TIME_DELAY

 

X1

  113  

X4

0–65,535

ALARM_ MESSAGE_ TEXT

   

X1

536

Character String

X4

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

COV_COUNT

   

X3

839

Unsigned

   

DEVICE_MAC_ ADDRESS

   

X3

3629

Unsigned

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X1

32581

Character String

X4

 

GRAPHIC_ ALIAS

   

X1

32623

Character String

X4

 

IN_TEST

   

X3

3368

Boolean

   

INSTANCE_ NUMBER

   

X

32589

Unsigned

   

INTRINSIC_ ALARMING_ DEFINED

   

X3

569

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

OFFLINE

   

X

913

Boolean

   

REMOTE_ DESCRIPTION

   

X3

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X3

538

Complex

   

REMOTE_ OBJECT_NAME

   

X3

2564

Character String

   

RESTORE_ COMMAND_ PRIORITY

   

X

721

Bit String

X

 

STATES_TEXT

   

X

931

Enumerated

   

STATUS

   

X

512

Enumerated

   

TRUNK_ NUMBER

   

X3

549

Unsigned

   

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Only present when intrinsic alarming is enabled.
2 Not writable in all instances.
3 Not present in all instances.
4 Only writable when intrinsic alarming is enabled.