Binary Input - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Binary Input

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

OUT_OF_ SERVICE

X

   

81

 

X

 

POLARITY

X

 

84

 

X

 

PRESENT_ VALUE

X

   

85

 

X1

 

PROPERTY_ LIST

X

   

371

     

ACTIVE_TEXT

 

X

 

4

     

ACTIVE_TIME_ RESET

 

X

 

114

     

ACKED_ TRANSITIONS

 

X2

 

0

     

ALARM_ VALUES

 

X2

 

7

 

X3

 

COS_COUNT

 

X

 

15

 

X

 

COS_TIME

 

X

 

16

     

DESCRIPTION

 

X

 

28

 

X

64 characters max

DEVICE_TYPE

 

X

 

31

 

X

 

ELAPSED_ ACTIVE_ TIME

 

X

 

33

 

X

 
EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X2

 

35

 

X3

 

EVENT_ MESSAGE_ TEXTS

 

X2

  351      
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X3 256 characters max

EVENT_TIME_ STAMPS

 

X2

 

130

     

INACTIVE_TEXT

 

X

 

46

     

NOTIFICATION _CLASS

 

X2

  17  

X3

1–4,194,303

NOTIFY_TYPE

 

X2

 

72

 

X3

 

RELIABILITY

 

X

 

103

 

X1

 

STATE_COUNT_ RESET

 

X

 

115

     

TIME_DELAY

 

X2

 

113

 

X3

0–65,535

ALARM_ MESSAGE_ TEXT

   

X2

536

Character String

X3

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

COV_COUNT

   

X

839

Unsigned

   

DEVICE_MAC_ ADDRESS

   

X

3629

Unsigned

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

IN_TEST

   

X

3368

Boolean

   

INSTANCE_ NUMBER

   

X

32589

Unsigned

   

INTRINSIC_ ALARMING_ DEFINED

   

X4

569

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

GRAPHIC

   

X2

32581

Character String

X3

 

GRAPHIC_ ALIAS

   

X2

32623

Character String

X3

 

OFFLINE

   

X

913

Boolean

   

REMOTE_ DESCRIPTION

   

X4

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X4

538

Complex

   

REMOTE_ OBJECT_NAME

   

X4

2564

Character String

   

SAB_MAC_ ADDRS

   

X

3645

Unsigned

   

SLOT

   

X

519

Unsigned

   

STATES_TEXT

   

X

931

Enumerated

X5

 

STATUS

   

X

512

Enumerated

   

TRUNK_ NUMBER

   

X

549

Unsigned

   

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Only writable when Out of Service is set to True.
2 Only present when intrinsic alarming is enabled.
3 Only writable when intrinsic alarming is enabled.
4 Not present in all instances.
5 Not writable in all instances.