Analog Value - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Analog Value

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

OBJECT_NAME

X

   

77

 

X

 

PRESENT_ VALUE

X

    85  

X

 

PROPERTY_ LIST

X

   

371

     

UNITS

X

   

117

 

X

0–65,535

ACKED_ TRANSITIONS

 

X1

 

0

     

COV_ INCREMENT

 

X

 

22

 

X2

any value > 0

DEADBAND

 

X1

 

25

 

X3

 

DESCRIPTION

 

X

 

28

 

X

64 characters max

EVENT_ DETECTION_ ENABLE   X          

EVENT_ENABLE

 

X1

 

35

 

X3

 

EVENT_ MESSAGE_ TEXTS

 

X1

  351      
EVENT_ MESSAGE_ TEXTS_ CONFIG  

X

     

X3

256 characters

EVENT_TIME_ STAMPS

 

X1

 

130

     

HIGH_LIMIT

 

X1

 

45

 

X3

 

LIMIT_ENABLE

 

X1

 

52

 

X3

 

LOW_LIMIT

 

X1

 

59

 

X3

 

MAX_PRES_ VALUE

  X

X

65

Real

X4

 

MIN_PRES_ VALUE

  X

X

69

Real

X4

 

NOTIFICATION _CLASS

 

X1

 

17

 

X3

1–4,194,303

NOTIFY_TYPE

 

X1

 

72

 

X3

 

PRIORITY_ ARRAY

 

X5

 

87

     

RELIABILITY

 

X

 

103

 

X

 

RELINQUISH_ DEFAULT

 

X5

 

104

 

X

 

TIME_DELAY

 

X3

 

113

 

X

0–65,535

ALARM_ MESSAGE_ TEXT

   

X1

536

Character String

X3

 

ALARM_STATE

   

X

1006

Enumerated

   

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0–249

COV_COUNT

   

X5

839

Unsigned

   

DEVICE_MAC_ ADDRESS

   

X5

3629

Unsigned

   

DISPLAY_ PRECISION

   

X

661

Enumerated

X

0–12

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X1

32581

Character String

X3

 

GRAPHIC_ ALIAS

   

X1

32623

Character String

X3

 

IN_TEST

   

X

3368

Boolean

   

INSTANCE_ NUMBER

   

X5

32589

Unsigned

   

INTRINSIC_ ALARMING_ DEFINED

   

X5

569

Boolean

X

 

ITEM_ REFERENCE

   

X

32527

Character String

   

OFFLINE

   

X

913

Boolean

   

REMOTE_ DESCRIPTION

   

X5

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X5

538

Complex

   

REMOTE_ OBJECT_NAME

   

X5

2564

Character String

   

RESTORE_ COMMAND_ PRIORITY

   

X

721

Bit String

X

 

STATUS

   

X

512

Enumerated

   

TRUNK_ NUMBER

   

X5

549

Unsigned

   

USE_COV_MIN _SEND_TIME

   

X5

3930

Boolean

X

 

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Only present when intrinsic alarming is enabled.
2 Not writable in all instances.
3 Only writable when intrinsic alarming is enabled.
4 For NCE, only writable for AVs on supervisory side, not on field controller side.
5 Not present in all instances.