Dynamically Creatable: No
Dynamically Deletable: No
|
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
|---|---|---|---|---|---|---|---|
|
OBJECT_NAME |
X |
77 |
X |
||||
|
OUT_OF_ SERVICE |
X |
81 |
X |
||||
|
PRESENT_ VALUE |
X |
85 |
X |
||||
|
PROPERTY_ LIST |
X |
371 |
|||||
|
RELINQUISH_ DEFAULT |
X |
104 |
X |
||||
|
UNITS |
X |
117 |
X |
0–65,535 |
|||
|
ACKED_ TRANSITIONS |
X1 |
0 |
|||||
|
COV_ INCREMENT |
X |
22 |
X |
any value > 0 |
|||
|
DEADBAND |
X1 |
25 |
X2 |
||||
|
DESCRIPTION |
X |
28 |
X |
64 characters max |
|||
|
DEVICE_TYPE |
X |
31 |
X |
20 characters max |
|||
| EVENT_ DETECTION_ ENABLE | X | 353 | |||||
|
EVENT_ENABLE |
X1 |
35 |
X2 |
||||
|
EVENT_ MESSAGE_ TEXTS |
X1 |
351 | |||||
| EVENT_ MESSAGE_ TEXTS_ CONFIG | X | 352 | X2 | 256 characters max | |||
|
EVENT_TIME_ STAMPS |
X1 |
130 | |||||
|
HIGH_LIMIT |
X1 |
45 |
X2 |
||||
|
LIMIT_ENABLE |
X1 |
52 |
X2 |
||||
|
LOW_LIMIT |
X1 |
59 |
X2 |
||||
|
MAX_PRES_ VALUE |
X |
65 |
X |
||||
|
MIN_PRES_ VALUE |
X |
69 |
X |
||||
|
NOTIFICATION _CLASS |
X1 |
17 |
X2 |
1–4,194,303 |
|||
|
NOTIFY_TYPE |
X1 |
72 |
X2 |
||||
|
RELIABILITY |
X |
103 |
X3 |
||||
|
RESOLUTION |
X |
106 |
|||||
|
TIME_DELAY |
X1 |
113 |
X2 |
0–65,535 |
|||
|
ALARM_ MESSAGE_ TEXT |
X1 |
536 |
Character String |
X2 |
|||
|
ALARM_STATE |
X |
1006 |
Enumerated |
||||
|
AUTHORIZA- TION_ CATEGORY |
X |
908 |
Enumerated |
X |
0–249 |
||
|
COV_COUNT |
X |
839 |
Unsigned |
||||
|
DEVICE_MAC_ ADDRESS |
X |
3629 |
Unsigned |
||||
|
DISPLAY_ PRECISION |
X |
661 |
Enumerated |
X |
0–12 |
||
|
ENABLED |
X |
673 |
Boolean |
X |
|||
|
EXECUTION_ PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
|
GRAPHIC |
X1 |
32581 |
Character String |
X2 |
|||
|
GRAPHIC_ ALIAS |
X1 |
32623 |
Character String |
X2 |
|||
|
IN_TEST |
X |
3368 |
Boolean |
||||
|
INSTANCE_ NUMBER |
X |
32589 |
Unsigned |
||||
|
INTRINSIC_ ALARMING_ DEFINED |
X4 |
569 |
Boolean |
X |
|||
|
ITEM_ REFERENCE |
X |
32527 |
Character String |
||||
|
OFFLINE |
X |
913 |
Boolean |
||||
|
REMOTE_ DESCRIPTION |
X4 |
32519 |
Character String |
X |
|||
|
REMOTE_ DEVICE_ADDR |
X4 |
538 |
Complex |
||||
|
REMOTE_ OBJECT_NAME |
X4 |
2564 |
Character String |
||||
|
RESTORE_ COMMAND_ PRIORITY |
X |
721 |
Bit String |
X |
|||
|
SAB_MAC_ ADDR |
X |
3645 |
Unsigned |
||||
|
SLOT_A |
X |
990 |
Unsigned |
||||
|
SLOT_B |
X |
991 |
Unsigned |
||||
|
STATUS |
X |
512 |
Enumerated |
||||
|
TRUNK_ NUMBER |
X |
549 |
Unsigned |
||||
|
USE_COV_MIN _SEND_TIME |
X |
3930 |
Boolean |
X |
|||
|
USER_NAME |
X |
2390 |
Character String |
X |
400 characters max |