Accumulator - Metasys - LIT-1201532 - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE85 Network Automation Engine - NAE45 Network Automation Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Product
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Accumulator

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

MAX_PRES_ VALUE

X

   

65

 

X

 

OBJECT_NAME

X

   

77

 

X

 

OUT_OF_ SERVICE

X

   

81

 

X

 

PRESENT_ VALUE

X

   

85

 

X

 

PROPERTY_ LIST

X

   

371

     

SCALE

X

   

187

 

X

 

UNITS

X

   

117

 

X

0–65,535

ACKED_ TRANSITIONS

 

X1

 

0

     

DESCRIPTION

 

X

 

28

 

X

64 characters max

DEVICE_TYPE

 

X

 

31

 

X

20 characters max

EVENT_ DETECTION_ ENABLE   X   353      

EVENT_ENABLE

 

X1

 

35

 

X2

 

EVENT_ MESSAGE_ TEXTS

 

X1

  351      
EVENT_ MESSAGE_ TEXTS_ CONFIG   X   352   X2 256 characters max

EVENT_TIME_ STAMPS

 

X1

 

130

     

HIGH_LIMIT

 

X1

 

45

 

X2

 

LIMIT_ENABLE

 

X1

 

52

 

X2

 

LIMIT_ MONITORING_ INTERVAL

 

X1

 

182

 

X2

 

LOGGING_ OBJECT

 

X3

  183      

LOGGING_ RECORD

 

X3

 

184

     

LOW_LIMIT

 

X1

 

59

 

X2

 

NOTIFICATION _CLASS

 

X1

 

17

 

X2

1–4,194,303

NOTIFY_TYPE

 

X1

 

72

 

X2

 

PRESCALE

 

X

 

185

 

X

 

PULSE_RATE

 

X1

 

186

 

X2

 

RELIABILITY

 

X

 

103

 

X4

 

TIME_DELAY

 

X1

 

113

 

X2

 

VALUE_ BEFORE_ CHANGE

 

X

  190      

VALUE_ CHANGE_ TIME

 

X

  192      

VALUE_SET

 

X

  191  

X

0–268,435, 455

ALARM_ MESSAGE_ TEXT

   

X1

536

Character String

X2

 

ALARM_STATE

   

X

1006

Enumerated

   

ANTI_SPIKE

   

X3

722

Boolean

X

 

AUTHORIZA- TION_ CATEGORY

   

X

908

Enumerated

X

0-249

COV_COUNT

   

X

839

Unsigned

   

DEVICE_MAC_ ADDRESS

   

X

3629

Unsigned

   

DISPLAY_ PRECISION

   

X

661

Enumerated

X

 

ENABLED

   

X

673

Boolean

X

 

EXECUTION_ PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X1

32581

Character String

X2

 

GRAPHIC_ ALIAS

   

X1

32623

Character String

X2

 

IN_TEST

   

X

3368

Boolean

   

INSTANCE_ NUMBER

   

X

32589

Unsigned

   

ITEM_ REFERENCE

   

X

32527

Character String

   

INTERNAL_ UNITS

   

X

3432

Enumerated

X

 

OFFLINE

   

X

913

Boolean

   

PERIODIC_ UPDATE

   

X

2192

Unsigned

X

 

REMOTE_ DESCRIPTION

   

X3

32519

Character String

X

 

REMOTE_ DEVICE_ADDR

   

X3

538

Complex

   

REMOTE_ OBJECT_NAME

   

X3

2564

Character String

   

ROLLOVER_ LIMIT

   

X3

823

Unsigned

X

 

SAB_MAC_ ADDR

   

X

3645

Unsigned

   

SCALED_ PRESENT_ VALUE

   

X

4694

Unsigned

   

SCALED_VALUE

   

X

4694

Real

   

SLOT

   

X

519

Unsigned

   

STATUS

   

X

512

Enumerated

   

TRUNK_ NUMBER

   

X

549

Unsigned

   

USER_NAME

   

X

2390

Character String

X

400 characters max

1 Only present when intrinsic alarming is enabled.
2 Only writable when intrinsic alarming is enabled.
3 Not present in all instances.
4 Only writable when Out of Service is set to True.