Networking Options - Metasys - LIT-1201532 - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE85 Network Automation Engine - NAE45 Network Automation Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Product
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09

Router 1, Clause 6:IP/MSTP MSTP/MSTP

   

Annex H, BACnet Tunneling Router over IP

   

BACnet/IP Broadcast Management Device (BBMD)

   
 

Does the BBMD support registrations by Foreign Devices?

Yes

No

 

Does the BBMD support network address translation?

Yes

No

1 The NAE8500 series device cannot be used as a router.