Character Sets Supported - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Product
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

ISO 10646 Unicode Transformation Format-8 (UTF-8)

IBM®/ Microsoft® Double-Byte Character Set (DBCS)

ISO 8859-1

ISO 10646 Universal Character Set-2 (UCS-2)

ISO 10646 (UCS-4)

Japanese Industrial Standard (JIS) X 0208