Product Description - Metasys - LIT-1201532 - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 9

NAE/NCE Protocol Implementation Conformance Statement

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Protocol Implementation Conformance Statement
Document number
LIT-1201532
Version
9
Revision date
2019-04-09
Language
English

The NAE/NCE is a component of the Metasys® system. In terms of the BACnet protocol, the NAEs/NCEs are building controllers and support many operator workstation services.

The NAE/NCE can monitor and supervise a network of BACnet and non BACnet devices. An operator views the data on a web browser that is logged on to the web-enabled user interface of an NAE/NCE. As a building controller, other BACnet devices on the network can read and write to the BACnet objects within an NAE/NCE.