Video Recorder points definition - Metasys - LIT-12013151 - System Integration - CCURE-Victor Integration - 10.0

NAE Commissioning for C•CURE-victor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > CCURE-Victor Integration
Document type
Application Note
Document number
LIT-12013151
Version
10.0
Revision date
2018-12-17

A single Video Recorder object is represented by one Metasys Device object:

Metasys object attribute

ID

SUB ID

Possible values description

(R)eadable (W)ritable

Point definition

 

Communication Status

20

0

Online (2) / Offline (1)

Linked to the status of the device

(This is not a physical MSEA point)

R

Alert Status

20

2

Unknown (1)

Normal (2)

Overheat (4)

Reboot (8)

LogRotate (16)

AlarmRecoveryCompleted (32)

SensorAlarm (64)

LockDown (128)

R

Storage Status

20

1

Unknown (0 or 1)

Normal (2)

NoVolumes (4)

VolumeMissing (8)

VolumeCorrupt (16)

VolumeFailed (32)

NewVolume (64)

VolumeReAdded (128)

UnhealthyDisk (256)

DiskTemperature (512)

RaidDegradation (1024)

Backup (2048)

DataCulling (4096)

DiskFull (8192)

R

Archive Storage Status

20

3

Unknown (0) / Normal (1) / Degraded (2)

R
Note: If the state of a recorder changes to online or offline, there is a two minute delay before the event is reported. If you configure Metasys alarms, keep this delay in consideration.