Inserting field devices and points into an SCT archive database from MCT - Metasys - LIT-12013151 - System Integration - CCURE-Victor Integration - 10.0
Building Automation Systems > Utilities and Integrations > CCURE-Victor Integration
Document type
Application Note
Document number
LIT-12013151
Version
10.0
Revision date
2018-12-17
About this task
If you use SCT to configure the integration, you can
transfer device and point information directly from MCT to SCT.
Procedure
In MCT, from the File menu, click Insert into SCT Database.
Enter a User ID and Password to
connect to SCT installed on the same computer.
Figure 1. Connecting to SCT from MCT
Click Connect.
Select the Archive database, then select the VND Integration.
Note: If the archive database does not include a VND integration, open the
archive in SCT and perform an Upload from the NAE copy the integration
object to the archive.
Click OK. The objects are created inside the selected
integration. If you chose to include Metasys UI objects, they are created
inside the ADS.