About this task
To create an offline database for the victor configuration, install the victor WS Config Tool on a PC that is on the same network as the victor server. Use the WS Config Tool to generate an XML file that contains the entire configuration. You can then use the XML file in MCT.
To install the WS Config Tool, complete the following steps: