About this task To create the offline database, first export the C•CURE 9000 configuration. Procedure Launch the C•CURE 9000 Administration Station software. From the Hardware tree view, select the cluster to export, right-click it and select Copy to. Figure 1. Start Data Export process Navigate to the desired location to save the file, enter a file name, then click Save. After the process completes, a confirmation message appears. Click OK. Use this XML file in the MCT. See Generating an MCT .imp file.